4/1/2010 4:18 PM | |
Posts: 5 Rating:
|
Hi, I want to know if it is possible to interface the 224XP PLC with a 4x16 Line LCD from http://www.matrixorbital.com/ . The LCD supports RS-232 communication, but my PLC is communicating with my computer via USB/PPI Multi-Master Cable. Can I use the other RS-232 port on the PLC to communicate with the LCD? Can I use the FreePort Mode on the PLC? Is there a link on how to do this? Thank you, |
7/7/2010 5:23 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
It will not work without any converter.. Because, as Helmut_13 said, PLC doesnot have any RS 232 port. So you must have to convert signal from RS485 to RS232, either using PC-PPI cable or by any converters... Regards, Devesh Vithani |
Last edited by: Vithani at: 7/7/2010 5:24 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on