(0)| 7/21/2010 4:30 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Yes ofcourse you can do this with the help of.. For this you need Profibus Module Also have a look at its manual and following thread for more on Profibus and MM440 communication.. Micromaster Profibus dp interface Regards, Devesh Vithani |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
| 7/22/2010 6:13 AM | |
|
Joined: 10/7/2005 Last visit: 1/21/2026 Posts: 3054 Rating:
|
Hello Yoga Shankar Vithani's sugestion is generally correct, but will only allow you to have the Drives on ONE CPU (they'll become so called unilateral I/O devices of the relevant CPU and are NOT part ofyour Software redundant system). If you need the drives to bepart of the Software redundant system, I'm afraid to say that you will have to gothe CP341 (to be located in a - redundant IM153 based- ET 200M Station). The only alternative I can see to this, is to go for an S7-400H system and use a Y-Link to link any non-redundant Profibus DP Slavesto it. I hope this helps |
|
Cheers |
|
This contribution was helpful to
|
|
| 7/22/2010 7:08 AM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
I gave this answer because Yoga Shankar has mentioned that he has two NON REDUNDANT Drives so what I think is, he is going to connect One drive to one CPU and another to another... Thats how its going to work' Devesh |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
| 7/28/2010 8:44 AM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Ok then you have to go for options suggested by fritz Devesh |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
Follow us on