10/12/2010 9:49 PM | |
Joined: 9/27/2006 Last visit: 9/4/2025 Posts: 12397 Rating:
|
Hello senthils; You do not mention the model of MM4 drive you want to operate. Hereare somecollections of manuals for different models so that you can choose what you require: Parameter lists for different models of MM4 drives: https://support.automation.siemens.com/WW/llisapi.dll?query=MM4+parameters&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8&cssearchengine=NEW Operation manuals for different models of MM4 drives: https://support.automation.siemens.com/WW/llisapi.dll?query=MM4+operatiion&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8&cssearchengine=NEW&x=23&y=6 In these operation manuals you should find sections on Motor Identification procedure, Inverter Protection, Thermal protection, Overload Response, Control mode selection(e.g. V/f, SLVC...), etc... Do you plan on controlling the drive using digital/analog signals from the PLC as described in these opertions ,manuals, or using a Profibus-DP optional communications board? Operating Instructions: MICROMASTER PROFIBUS Optional Board Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/12/2010 9:52 PM |
|
10/14/2010 11:04 AM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, please see this link if it can help you decide which MM4 to use Regards, Graeme
|
Follow us on