11/9/2010 12:42 AM | |
Posts: 18 Rating:
|
Tane, I too am looking for information for the OP1S. I have 7 units that are locked out and the display is mostly in German, I need English. I have a display the reads ON Locked and the PMU has status 008. I have not been able to find ANY information on this unit except that it is in the phase out A/O 10-1-2010. Splitted from I need manual for OP1S 6SE7090-0XX84-2FK0. |
Last edited by: O_Moderator at: 11/10/2010 12:37 PMnew subject after splitting |
|
11/9/2010 7:06 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, It depends what kind of drive you have there. (concerning parameters). For example if you have Masterdrive VC: look at http://support.automation.siemens.com/WW/view/en/13472409 (Chapter 5). There you will see how to navigate with parameters using OP1S panel. To change it language - P060=7 and P050=1. BR, Hristo Mihalev |
Follow us on