10/27/2006 10:10 AM | |
Posts: 1084 Rating:
|
Is there still a question in this? cause the answer is in there as well. with regards, ikkezelf |
10/27/2006 1:37 PM | |
Posts: 1275 Rating:
|
I have been wondering the same thing... [:)] TSC, could you please clarify your question? Best regards, Danielle |
10/28/2006 12:08 AM | |
Joined: 5/19/2006 Last visit: 8/21/2025 Posts: 550 Rating:
|
Even though this seems to be the definition of Lifebeat monitoring timers, in facts there are different schemas in sending out the packets to the PLC by WinCC S7Channel & SINEC Drivers (ISO or RFC1006). One set of Lifebeat monitoring timers are running at the SINEC driver level (ISO = 10s AK , RFC1006 = 30s Keep – Alive) independent of WinCC S7Channel. These messages are designed to ensure lower transportlayer heartbeat and are configured with SIMATIC NET.
AttachmentLBM-S7ChannelTCP.zip (442 Downloads) |
Last edited by: Dec at: 10/28/2006 5:36 AMLast edited by: Dec at: 10/28/2006 12:32 AM |
|
10/28/2006 1:14 PM | |
Posts: 3149 Rating:
|
Hi I think TSC just intended to share his experiences/knowhow with other users [:D] nemo |
Follow us on