10/30/2006 12:03 PM | |
Posts: 25 Rating:
|
Dear salma, I apologisefor the delayed reply. Basically i'm confused of the various Database files found in the Project folder of the WinCC.[:blush:]. Clarification N0 1: When i created an empty project, the Project folder Creates Data base files 1.<Project name> 2,048 KB 2.<Project name>10,240 KB 3.<Project nameRT> 2,048 KB 4.<Project nameRT> 10,240 KB What are these DBFiles?? Why they are created twice with two different sizes 2MB and 10 MB?? Clarification N0 2: In the same project if i create taglogging then it creates 1.<Project nameTlg> 1,024 KB 2.<Project nameTlg> 51,200 KB 3.Common archiving folder 4.Archive manager folder. What are these DB Files??Why they are created twice with two different sizes 1 MB and 51MB. What is that Archive manager folder which has the tag logging fast and Taglogging slow DB files?? I have attached the screen shots of the project folder in either cases. Please clarify me. AttachmentProject folder after taglogging enabled at computer prop.,.zip (435 Downloads) |
Follow us on