1/21/2011 8:12 AM | |
Posts: 739 Rating:
|
hi, i need help to configure a mm 430 160kW please see: Getting Started Guide: MICROMASTER 420/430/440 Operating Instructions: MICROMASTER 430 7,5 kW - 250 kW Parameter List: MICROMASTER 430 How to command the inverter with Drivemonitor(which PM is necessary to use Drive monitor for running the motor). Pls. use a PC-Inverter-connection kitt = 6SE6400-1PC00-0AA0 (see also page 21 in GSG) And how increasing the sp value with bop-2 in manual mode.see chater 3.2 OPI |
Follow us on