(0)| 2/4/2011 7:16 AM | |
|
Posts: 11 Rating:
|
Dear Sir, I am a novice when it comes to SIEMENS.I have an H-System that hastwo ET 200M.I want to read the Diagonistics of DP Master.Since i have two et200,each will have a different diagonistic address.Now what i want to ask is that where do i put the respective diagonistic address in the sample program.Does it pick up the address by itself?.I know in sfc51 we put the diagonistic address in index but here it is write protected. Splitted from Question - How to detect a modul failer of an ET200M within the DP-Master. |
Last edited by: O_Moderator at: 2/4/2011 9:33 AMnew subject after splitting |
|
| 2/4/2011 9:49 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Look at How do you find out the status of the stations of a DP master system or of a PROFINET IO system? But if the CPU is write protected with password you will need it in order to download this logic.Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 2/4/2011 9:49 AM |
|
Follow us on