(0)| 2/9/2011 1:44 PM | |
|
Joined: 3/21/2006 Last visit: 1/23/2026 Posts: 10248 Rating:
|
Hello, STEP 7 V5.5 + PC Adapter USB 6ES7972-0CB20-0XA0. I suggest you to buy STEP 7 Professional 2010 instead of 'only' Step7 5.5. Best regards, Hristo Mihalev |
| 2/9/2011 1:58 PM | |
|
Joined: 8/31/2005 Last visit: 12/16/2025 Posts: 2198 Rating:
|
Hello, the actual version of STEP 7 is V5.5. If your CPU has a PN interface you can use any Ethernet card to connect. All CPUs have a MPI connector, to use it you need a CP5711 (USB)a CP5512 (PC Card) or a PC Adapter USB (only up to 1,5 MByte/s) Or you buy a Field PG, there you have it in one (Laptop, CP5612 (built in version of CP5512), programmer and Software) and ready to run! There is a configurator for the PG M3 (select country, klick on configurators and then on"SIMATIC Field PG M3") |
Last edited by: miami at: 2/9/2011 2:01 PMLast edited by: miami at: 2/9/2011 2:01 PM |
|
| 2/10/2011 5:56 AM | |
|
Posts: 27 Rating:
|
SIMATIC S7, STEP 7 V5.4 SP5 Order No. 6ES7810-4CC08-OYA5 SIMATIC PC ADAPTER Type: 6ES7972-0CA23-0XA0 |
Follow us on