(0)| 4/22/2011 2:57 AM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello jirimatus; I would suggest you look at this thread: /tf/WW/en/Posts/21822 jmj's postingcontains a very interesting link, it could be what best suits your application. Hope this helps, Daniel Chartier |
This contribution was helpful to
|
|
| 4/25/2011 10:16 AM | |
|
Posts: 642 Rating:
|
Hi, I would convert the S5 controller to Profibus (IM308C). Then you only have to plug the Profibus and motion control wires. If you need a IM308C - i have it in stock. You also can rent it. Regards
André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
| 4/25/2011 3:52 PM | |
|
Posts: 12 Rating:
|
One other option less expensive than the Phoenix modules is contained in the attachment. These adapters are manufactured by Siemens. I have used these in the past and will satisfy your need to be able to switch quickly between the S5 and S7 system. AttachmentS5-to-S7_IO_Adaptesr_08222008.pdf (491 Downloads) |
Follow us on