6/27/2011 7:14 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Perhaps we will return to "CPU is demage" again. |
6/27/2011 7:36 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Dear UMENCHO, i have only Simatic Filed PG M2 with me. If CPU is damage, is there any way we can resolve it? i alsoChecked CPU healthyness by removing CPU form rack. i have given external 24 V DC Supply to one of theCPU with Connecting fiber optic link with another cpu. Also taken out front connecter of CPU I/o's ,EPROM and backup battery. But during power on CPU stop led continuos flashing? What could be the reason? i mean Power fail or Power surge? |
VANDE MATARAM..... |
|
Follow us on