7/14/2011 11:51 AM | |
Joined: 6/13/2009 Last visit: 6/15/2025 Posts: 26 Rating:
|
Dear All, i am facing problem withSinamics G120 with CU-230-p HVAC + PM240. i am using this drive for Compresor Application. It abruptly gives OverSpeed Fault. i tried to change speed hysterises parameter P2162 but its not getting increases above 10% of the Motor rated RPM. By default it is set to 10% of rated Motor RPM. Same parameter i have seen in MM440 but its default in MM440 is 20Hz. Sinamics G120 has same Plateform of Parameters as MM440 but i am not finding root cause for Overspeed Fault. Can any one help me for theCU-230-p HVAC, as i am new to this control Unit ? I am attaching Parameter backup with this Thread. Thanks in advance. Anakin AttachmentComp_app.zip (402 Downloads) |
7/25/2011 8:03 AM | |
Joined: 6/13/2009 Last visit: 6/15/2025 Posts: 26 Rating:
|
Nobody has worked on CU230-p-HVAC???????????????? |
Follow us on