9/27/2011 11:46 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, regarding to your inquiry, perhaps it could be mainful for you the download of the example S-SCL-Program (link): http://support.automation.siemens.com/WW/view/de/19362106 With best regards |
9/27/2011 8:40 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Dear Tyhoon [code] Best regards AttachmentHd21___1.zip (270 Downloads) |
Last edited by: hdhosseini at: 9/28/2011 5:43 AMLast edited by: hdhosseini at: 9/27/2011 8:42 PM//Attachment added |
|
9/28/2011 3:59 AM | |
Joined: 9/1/2010 Last visit: 8/29/2025 Posts: 27 Rating:
|
Thanks for the help guys, I think I will use the Array of Bools method as this is a function block that i want to create instances of. Ps hdhosseini the last if statement for test 5 should be "IF((hd)AND(dw#16#10))..." I had problems when investigating your code. But i am a newb so it was good to exercise referencing using the hex memory address. Thanks |
Follow us on