10/3/2011 2:30 PM | |
Joined: 10/7/2005 Last visit: 9/3/2025 Posts: 3049 Rating:
|
Hello Ahmed I'm afraid to say you can NOT use your IM308B (6ES5 308-3UBxx) with the S120 (unless you'll find a COMET200 useable typefile for it) and will need to use an IM308C (6ES5 308-3UCxx)together withCOM Profibus V5.x for the configuration. Below area few links with more on this and I hope it helps: Configurable DP-slaves for IM 308B What are the differences between the DP master interface IM 308-B and the successor product IM 308-C? ET 200 Distributed I/O System with IM 308-C manual |
Cheers |
|
This contribution was helpful to
1 thankful Users |
10/4/2011 11:56 AM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
closed cause question posted twice. The second thread with the subject Communication of S120 Drives with S5 PLCis published within the conference SINAMICS. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on