10/4/2011 12:07 PM | |
Posts: 103 Rating:
|
Dear all, How are you, I have Step5 system connected to SCADA COROS LSB through (HIRSCHMANN ASGE 2E AC) , this device convert from fibre optic (PLC Side) to serial (PC Side) , the client wants to upgrade from COROS to Wincc , I have researched in PDFs , I found out PDF in the attachment describe how to connect wincc to S5 through serial 3964R my questions are , can I use built-in serial port in new PC Station? or should I purchase special serial card? -------- Does wincc include any tool to convert COROS Sw to Wincc Sw Directly? thanks in advance ------- in this system I have 2 stations Master and Forward Wincc should be installed on both, I need 10000 Tags license what's suitable ًwincc order number? -------- AttachmentS5Serial3964R.pdf (424 Downloads) |
Last edited by: ahmedmae94 at: 10/4/2011 2:20 PMLast edited by: ahmedmae94 at: 10/4/2011 1:40 PMLast edited by: ahmedmae94 at: 10/4/2011 1:31 PMLast edited by: ahmedmae94 at: 10/4/2011 12:50 PMLast edited by: ahmedmae94 at: 10/4/2011 12:33 PM |
|
Follow us on