10/20/2011 7:23 PM | |
Posts: 50 Rating:
|
I am trying to writ a SCL program to transmit ASCII data to a CP 340. I have a CPU315-2 PN/DP. I have declared a DATA BLOCK at the very top of OB1 (See attached file). I would like to fill the array with ASCII data. I would like transmit the data in ASCII to a CP 340. The attached file shows what I have written but I am having problems compiling the file, I get an error. Any help that can be provided would be appreciated. Attachmentcp 340 prg.pdf (261 Downloads) |
10/21/2011 10:20 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread Communicating with CP-340 PtP using SCL. Best regards O_Moderator |
Follow us on