11/29/2011 9:13 AM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Dear Strongs Looks like you have a S5 130 system. They were programmed with PG 630. I have attached a Manual of the S5 130 system. Unfortunately it is only in German. These PLCs did not a PG port on the CPU. Instead there was a seperate 511 PG module installed in the rack. You should be able to go online using a PG with TTY port and 15Pin to 25Pin adaptor cable. If you do not have the PG card installed, then the only option may be to take out the EPROM and read the contents using a EPROMMER. Good Luck !! Cheers Navnag AttachmentS5-130K_Manual.pdf (419 Downloads) |
There is no such thing as the last bug in a program |
|
Follow us on