1/5/2012 11:37 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello I think so that you can use the FB42 "CONT_S". This FB has two outputs, QLMNUP (Typ: bool) for Manipulated signal up and QLMNDN for Manipulated signal down. Please see the informations of the online help for description of function and the input parameters. Further informations you will find in the FAQ: http://support.automation.siemens.com/WW/view/de/18459342 With best regards |
Follow us on