(0)| 2/1/2012 8:20 AM | |
|
Posts: 6 Rating:
|
Hi, I need to modify a HMI which has a Sm@rtAccess license and will involve an OS update. I assume this will wipe other stuff including the Sm@rtclient / Access license. Does the license reside on the actual HMI hardware and can it be removed/re-installed with a USB stick or other medium following an OS update? |
| 2/1/2012 9:54 AM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9106 Rating:
|
Hello, Before you perform an OS update, you should remove the license from panel Here is a link: What should you watch out with regard to licenses for WinCC flexible and panels? After removing the license from panel, you can perform an OS update. Then you will have to transfer project again and you have to tranfer license to panel. Best regards, Wizard |
Follow us on