(0)| 2/2/2012 2:44 PM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello, The Problem is not in the *.gsd file of the panel. It is in the version of your WinCC flexible. You have to use WinCC flex. 2008 SP2 UPDATE 13 / SP3.
AttachmentWinCC_flexible_Version_e.zip (178 Downloads) |
|
Ayman Elotaify |
|
| 2/2/2012 3:31 PM | |
|
Posts: 123 Rating:
|
Hi All, I am using WinCC flex 2008 sp2 Upd4, it must be ok i guess. Step7 5.5+sp1 distributed safety 5.4+sp5 I need this GSD in HW config in order to configure the profisafeV2 telegrame address and time of response. when i integrate the WinCC app in S7 : 1 HMI object is added in NetPro, nothing in HW so if I add the needed gsd in HW conf : then i have 2 HMI object in NetPro it is like if the HMI gsd in HW conf is not a communication partner for the WinCC apps I am even able to make a siemens demo software running with few modification. with this conf : CPU317F 2PN/DP, D-link Wifi Access point, MP277F iwlan v2 but to create my own HWconf and NetPro conf , it seams problematic. please see attachement (2 print screen)
AttachmentPrintScreen.zip (255 Downloads) |
Last edited by: S44 at: 2/2/2012 3:40 PM |
|
| 2/2/2012 3:46 PM | |
|
Joined: 9/28/2005 Last visit: 12/9/2025 Posts: 2957 Rating:
|
Well I can't really see what is the problem, but please check this link Which GSDML files are there for the operator panels for Profinet IO? |
|
Best regards, |
|
| 2/2/2012 3:50 PM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello, Check the picture. And try with your software version and tell us, do you found the panel in WinCC flex or not? If not, then update toWinCC flexible 2008 SP2 Update 13.
|
|
Ayman Elotaify |
|
| 2/2/2012 4:34 PM | |
|
Posts: 123 Rating:
|
hello, i was able to this this panel in wincc flex with sp2 upd4, now i am with sp2 upd13! still same problem
|
Follow us on