(1)| 6/26/2012 2:11 PM | |
|
Joined: 12/20/2008 Last visit: 9/3/2025 Posts: 556 Rating:
|
Two places a digital output or databit is written. Two places equal to instruction is used for the same output. |
| 6/27/2012 6:45 AM | |
|
Joined: 10/7/2005 Last visit: 1/14/2026 Posts: 3054 Rating:
|
Hello Lucky123 X-ref has some usefulfilter functions which makes it easy to spot double assignments and also comes in handy to for example find out if an Timer or Counter has accidentally been double assigned. All you have to do is to open the Filter dialogue in the X-ref, select the type of address (e.g. Outputs)and then either useselection number 7 to only disaply multiply "=" assignments or number 2 if you also want to have for example "Set/Reset" assignments displayed. Attached is a pic which should help in make sense out of the above. |
|
Cheers |
|
This contribution was helpful to
|
|
| 6/27/2012 11:13 AM | |
|
Joined: 12/20/2008 Last visit: 9/3/2025 Posts: 556 Rating:
|
Fritz, That really helped. I found three more double coil in my program, which I would have otherwise found while running the sequence eventually. Thanks a lot for letting me know this,earlier Daniel also mentioned the same, but I did really not know about point number 7, until you posted out the solution. Thanks once again. As always, Cheers! :) |
This contribution was helpful to
|
|
Follow us on