9/25/2012 5:02 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Please have a look at: What transfer options are available in the various operator panels? And the Manual. Regards, Marcjan |
Last edited by: Marcjan at: 9/25/2012 5:06 PMProblem solved? |
|
9/26/2012 11:54 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello Sarris, Your Field PG has a COM port (It is the one with 25 pins, called Com1/TTY) To use the cable you have, you need the (25-pin to 9-pin) adapter, which was a part of delivery of your Field PG. Have a look at the following link: Where can you obtain a 25-pin to 9-pin adapter (gender changer) for the Field PG, Field PG M and Field PG M2? (It is possible to make your own.) Best regards, Wizard |
9/26/2012 5:48 PM | |
Posts: 5 Rating:
|
Thanks for the help Wizard. What if I want to use my PC for the download. Should I use a USB-to-serial adapter to connect this cable? Regards |
9/27/2012 9:42 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello Sarris, |
Follow us on