3/22/2013 9:02 AM | |
Posts: 16 Rating:
|
Thank you for your reply, I have configure a DP/DP coupler version 2 in the comprofibus and export the entire e configuration as binary file and download the binary file in the CP50M0 using ss52com software.But the DP/DP coupler still shows a steady busfault...as if it cannot read the master.All terminating resistance of the profibus connector are properly configure e in the both sides of the cable . Can you suggest me what else I have to do to healthy the bus fault.Also after downloading my configuration I am getting an error 4 at the output ECO of the block @PRODP.I also attached the *.2bf file which may help you to understand my configuration. Thanks for your help Best regards, Aniket AttachmentLSDCDRV_modi.zip (317 Downloads) |
Follow us on