6/13/2013 3:08 PM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
You have to write/send between s7200 and 300. In PCS7 you can then use blocks from the "standard library" like GET, PUT, SEND to write/send between s7400 and s7300 Check which you require, there are multiple blocks you can use for communication with s7300 edit: s7200 is not supported by pcs7, but dont know you can still use it in your network... |
Last edited by: Oreca at: 6/13/2013 3:10 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on