6/19/2013 10:30 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, Here there is an sample program to read the IO Device name with the block “Get_Name” TIP: The parameter STATION_NR should match with the property of the IO Device (Device View – properties – PROFINET interface [X1] - Etherent Address – PROFINET – Device Number). The device name could be monitored directly in Watch Table. AttachmentDIAG_Get_Name.zip (1040 Downloads) |
Last edited by: O_Moderator at: 6/20/2013 7:45 AMDenilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
Follow us on