6/29/2007 8:01 AM | |
Posts: 3 Rating:
|
I would like to archive in Historian the WinCC TLS tags coming from 2 sets of Redundant PCS7 V6.1OS servers. Refer to the system architecture in enclosed PDF. As far as I know, an OS client in PCS 7 keeps track of the redundancy aspect. However, an OS Client can be client to only 1 set of PCS 7 redundant server pair. Thusif I install an OS client in Historian, I can grab data from 1 pair of server only. My dilemma is how to get data from the second pair of redundant server. Also I would like to know how to interface with the OPC-HDA of PCS 7 V6.1. Any help is welcome AttachmentHistorian.pdf (653 Downloads) |
Follow us on