(0)| 10/2/2013 12:51 PM | |
|
Joined: 9/23/2005 Last visit: 1/19/2026 Posts: 4449 Rating:
|
Hi, one of the innovations of the SP1 for STEP7 V12 (Released for Delivery at http://support.automation.siemens.com/WW/view/de/76276623) is the possibility to use FBs, FCs and PLC User defined types as library types. With this, it is possible to centralize changes and control versions. |
|
Denilson Pegaia |
|
| 10/2/2013 12:58 PM | |
|
Joined: 9/23/2005 Last visit: 1/19/2026 Posts: 4449 Rating:
|
To add a block to a Project library as Type, it is just necessary to drag and drop it. The follow cast shows how to do it. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\01 creating.zip (492 Downloads) |
|
Denilson Pegaia |
|
| 10/2/2013 1:01 PM | |
|
Joined: 9/23/2005 Last visit: 1/19/2026 Posts: 4449 Rating:
|
To edit a block save as Type you need to use the menu option “edit type” ether in the Project tree or in the library. The follow cast shows how to do it. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\02 open editing mode.zip (428 Downloads) |
|
Denilson Pegaia |
|
| 10/2/2013 1:03 PM | |
|
Joined: 9/23/2005 Last visit: 1/19/2026 Posts: 4449 Rating:
|
After editing, it is interesting to check the consistency. For the changes be accepted is necessary to release the version. If you give up to use it is necessary to discard the changes. By release version you can specify a new version number and (optionally) set to deletion of old version of the block. Once released, you can upgrade projects or libraries. The follow cast shows how to do it. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\03 finishing editing.zip (375 Downloads) |
|
Denilson Pegaia |
|
| 10/2/2013 1:06 PM | |
|
Joined: 9/23/2005 Last visit: 1/19/2026 Posts: 4449 Rating:
|
If you don’t want more that the project block would be connected to the Type lib, you can give the command to “termination connection to type”. The follow cast shows how to do it. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\04 terminating.zip (330 Downloads) |
|
Denilson Pegaia |
|
| 10/2/2013 1:08 PM | |
|
Joined: 9/23/2005 Last visit: 1/19/2026 Posts: 4449 Rating:
|
To add a block to a Global library as Type it is just necessary to drag and drop it from the Project Library. It is not possible to drag&drop it directly from the project tree. The follow cast shows how to do it. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\05 global lib.zip (401 Downloads) |
|
Denilson Pegaia |
|
| 10/2/2013 1:09 PM | |
|
Joined: 9/23/2005 Last visit: 1/19/2026 Posts: 4449 Rating:
|
To add a block from a global library as Type, it is just necessary to drag and drop it. The follow cast shows how to do it. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\06 global lib to prject.zip (415 Downloads) |
|
Denilson Pegaia |
|
| 10/2/2013 1:18 PM | |
|
Joined: 9/23/2005 Last visit: 1/19/2026 Posts: 4449 Rating:
|
If you actualize a project from a global library, the project library is updated automatically The follow cast shows how to do it. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\07b lib to project.zip (415 Downloads) |
|
Denilson Pegaia |
|
Follow us on