10/17/2013 6:37 AM | |
Posts: 94 Rating:
|
Dear sir, I have upgraded the simantic manager v5.5 sp2 to sp3. upgradation completed successfully.but when i open the proect and tray to browese it some directory it shows out of memory popup. when i ok it it shows the the blank directory for browse,but after putting the path of the project it simantic manager close automatically. i already cleared the cache memory and s7project directories.please find the snaps for better clarification.help me it's an urgent. thank you in advance.
Attachmentsimantic_manager_v5.5.3.pdf (212 Downloads) |
10/17/2013 7:28 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, What OS you have installed on the PC? Check : What are the requirements for installing STEP 7 version V5.5? Compatibility list Regards, Marcjan |
Problem solved? |
|
10/17/2013 7:33 AM | |
Posts: 94 Rating:
|
I installed windows xp sp3....previously it was working with step7 v5.5 sp2. |
10/17/2013 7:47 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Check the other requirements, like memory. If that's o.k. try to repair the installation(insert disk en choose repair), if that doesn't work i suggest a -> Support Request. Regards, Marcjan |
Problem solved? |
|
Follow us on