9/30/2013 2:07 PM | |
Joined: 10/21/2012 Last visit: 10/11/2022 Posts: 10 Rating:
|
Dear All, Configuration- CU-320-2DP Double motor module. 90 KW motor(Each). Please suggest me the operating modes of two motors, used for the extruder application. Application critality is to synchronise the motors, and in case of any connecting gear break extruder blades must not come into contact means motors should stop safely, otherwise blades can be damaged. Please suggest me the safety interlocks that must be taken care in drives.
AttachmentExtruder_Drawing.pdf (170 Downloads) |
Follow us on