(0)| 11/28/2013 9:03 PM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Its not possible to create copies...however.. you can do this: Take a block icon from the template.pdl. It shows the same block icons, only they are not automatically generated. You can manually connect this icon to the structure of the temperature monitoring block... This block is not updated during the create/update block icons... You can however create just copy of the cfc chart, but that's not very a neat thing to do... |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on