7/16/2012 5:59 PM | |
Posts: 6 Rating:
|
Hi Karl, Here are the links to the Motiflex e100 drive and the baldor encoder http://www.baldor.com/support/literature_load.asp?ManNumber=MN1952 Encoder http://www.baldor.com/support/literature_load.asp?ManNumber=MN1943 Motiflex e100 Also attached is our interface diagram between the 802C and the blador drive AttachmentScan_Doc0077.pdf (94 Downloads) |
7/17/2012 6:16 PM | |
Posts: 6 Rating:
|
When you put the 802C in run mode from the computer is that simulation mode? Or is that the actual run mode?
|
3/12/2014 8:42 AM | |
Posts: 340 Rating:
|
new question is splittet to install 802c controller, 2 old dc motor and drive |
Follow us on