4/21/2014 5:56 PM | |
Joined: 1/15/2009 Last visit: 8/11/2025 Posts: 316 Rating:
|
Hi moneymike, That certainly is a tall order. The first things I would recommend for learning would be an in-class PCS 7 training. Short of that you can read the PCS 7 On Tour book which lays out a path to learn the basics in 10 days (albeit full time). If you do not have the PCS 7 On Tour Book then please read the PCS 7 Compendium Part A- Configuration Guidelines. This manual does a good job of walking through the setup and configuration of a PCS 7 Project. You can download and read that here,http://support.automation.siemens.com/WW/view/en/63187279 I would also recommned that you use this link as your start for all PCS 7 information (http://support.automation.siemens.com/WW/view/en/63481413). FAQs, manuals, application examples.. etc can all be found here. Goodluck!!!
|
The best location for all PCS 7 content (manuals, guides, application notes, FAQs, and videos). |
|
This contribution was helpful to
1 thankful Users |
Follow us on