5/22/2014 9:37 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
Hello, first you should check your motordata`s - not only the commutation angle. At commissioning I recommend to make a stationary measurement (if possible a rotary measurement too). What is the exact meaning of the motorparametes, you will find there: http://support.automation.siemens.com/WW/view/en/79690594 Does the temperature modell works (correct)? I don`t know your motor, so maybe the motor wight is not correct or it is a special motor with a special cooling. Do you get a motor temperature in r35? Does it fit to your motor? I suppose the resistance is not correct (when your motor is not correct). Zako |
Last edited by: GrasserF at: 5/23/2014 7:32 AMlink edit, de/en |
|
Follow us on