12/22/2005 12:45 PM | |
Posts: 102 Rating:
|
I' ve some problems with the printing of some reports. I have many actions written in C-Editor: every single action compiles many strings with the tags that I have in my project. These strings are internal tags that I use in a report created with the Report designer. After I compiled the strings my script launches the RPTJobPrint() of the relative report. The problem is that during the execution of the actions the system slow down, the I/O field are not refreshed, for example, and when the report come out from the printer I have that some fields of the report are empty. I attach to this message one of these actions that I wrote Thanks for your help. Best Regards. Attachmentpas.zip (847 Downloads) |
12/23/2005 12:38 PM | |
Posts: 102 Rating:
|
Thanks for your suggest. It was very helpful; modifying the script I resolved the problem and now the system works correctly. |
12/23/2005 1:30 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Glad to be of help. Happy holidays ! |
Follow us on