6/17/2014 4:51 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, which data`s do you have from the motor ? Only the name plate - is it an asynchornous motor? Otherwise, following the definition, how SINAMICS understand the motordata`s: http://support.automation.siemens.com/WW/view/en/79690594 But normally I do a statory and rotarymeasurement and a automatic speed controller optimization in VECTOR p1300 = 20 /21 (for asynchronous motors). |
With best regards, |
|
This contribution was helpful to
2 thankful Users |
Follow us on