6/24/2014 4:54 AM | |
Posts: 2348 Rating:
|
What you have in Setting PC-PG interface? |
6/25/2014 9:32 PM | |
Posts: 2 Rating:
|
It is possible to change a PC/PG mode both from the simulator and from The setting PC/PG interface placed in the Step 7 directory. In the past I've used two modes PLCSIM(MPI) or PLCSIM(profibus) and they've worked correctly. A local Siemens representative said that Service Pack 4 should solve my problem, but unfortunately after update a situation is the same as before. I've prepared several screenshots from my Step 7 environment, to show more precisely the whole problem. AttachmentPLCSIMProblem.zip (597 Downloads) |
6/26/2014 4:09 PM | |
Joined: 11/15/2006 Last visit: 3/26/2025 Posts: 1319 Rating:
|
Select PLCSIM(profibus) as the PLC has a profibus interface, that's what I suggest first. |
Have Fun! |
|
Follow us on