10/9/2007 2:07 AM | |
Posts: 6 Rating: (0) |
Hi Friends, I have built a simple step controller to increase or decrease the number of compressors energised based on an up and down signal using 2 digital inputs. The logic adds compressors in numerical order. I want to improve over the design by choosing to run the compressor which has been off the longest when stepping up and choosing to stop the compressor which has been running longest when stepping down in an effort to even out run hours. I have pondered for hours on how to do this in LOGO! any suggestions would be welcomed. Thanks in advance, Ant AttachmentSTEP CONTROLLER.zip (989 Downloads) |
10/9/2007 4:56 AM | |
Posts: 191 Rating: (58) |
Hi!! this is not an easy one.... i´m sorry i used a lot M´s, this is just an example... i´m counting time in seconds B005 when you press I1 the Q with less time ( which is not on )wil turn on when you press I2 the Q with more time ( which is on ) will turn off i know it is hard to follow, please study it and feel free to post any question. ROSA AttachmentSTEP CONTROLLER II.zip (998 Downloads) |
10/9/2007 7:42 AM | |
Posts: 2930 Rating: (432) |
Hi, you can find an example in the Siemens Internet pages. Here is a link: https://www.automation.siemens.com/logo/html_00/pdf/Gleichmaessiges_Auslasten_von_3_Verbrauchern.pdf It is created for 3 pumps. i hope this helps. Regards Helmut |
10/9/2007 9:46 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580) |
Hello, thanks ROSA for your very fast solution - the way is the same as in my opinion. So i can work at some details, because the SIEMENS-solution is only very easy and not what Ant_the_fridge want... Look at the attachement...... Best regards Betel AttachmentSTEP CONTROLLER_V3_4.zip (1009 Downloads) |
Last edited by: Betel at: 10.10.2007 01:11Add V4 with safe some funktion units and add some ideas. ==> Meine TAG-Listen: "deut." |
|
Follow us on