6/29/2010 6:55 AM | |
Posts: 28 Rating:
|
Dear Sir, Thank you very much for your help. I have just uploaded system config on you request. Please advise me. Thanks again. Attachmentsystem config.pdf (645 Downloads) |
6/29/2010 10:11 AM | |
Posts: 103 Rating:
|
Dear Yoona, Hi with the details given by you it includes H-sync module hence its S7400H system. Hence no software Redundancy is required. AlsoCP1613 is an ethernet card of siemens which is used for communication with redundant PLC's i.e. S7 400 H system. once installed in the PC along with the License for redundancy i.e. Red Connect. you dont needto configure redundancy in the Wincc. You are then allowed to make a fault tolerant connection of WInccto the H-System. I dont think that is considered in your configuration. Also find the details of the CP1613 card in the document attached. Please let me know if this card is considered in the project. Please revert back in case of any clarifications required. Attachmentin_cp1613_x.pdf (589 Downloads) |
Last edited by: PPND at: 6/29/2010 10:21 AMLast edited by: PPND at: 6/29/2010 10:20 AM |
|
11/4/2014 8:43 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
|
Follow us on