(0)| 11/7/2014 1:29 PM | |
|
Joined: 8/14/2013 Last visit: 7/22/2025 Posts: 16 Rating:
|
Hello, I have a similar problem. Have to communicate with ET200SP CM PtP to other vendor as a Modbus master with 7 databits and 1 stop bit. Was this problem solved somehow? To me it seems that user cannot define the databits and stop bits for Modbus anymore with these new logic controllers...
----------------- New subject after splitting from Modbus communication via ET200S CM PtP module. |
Last edited by: Min_Moderator at: 11/7/2014 2:44 PMSplitted |
|
| 11/11/2014 7:20 AM | |
|
Joined: 3/20/2013 Last visit: 1/20/2026 Posts: 676 Rating:
|
Yes, you are right. These changes are not possible over Modbus_Comm_Load. |
|
Best Regards, |
|
Follow us on