12/27/2014 12:17 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello Ricky_J, You have "6ES7416-2XN05-0AB0" installed on your system and the offline project contains "6ES7416-2XK02-0AB0" .First , do a comparison to see do you have any difference in your blocks folder. "System data" is part that stores data related to HW.Config. If you overwrite the offline project to the CPU, it enters the STOP mode and perhaps wrong data relatedto old CPU are saved in actual CPU and your system never runs with that.
I am thinking of 2 options. First, upload the online working project , then add blocks to that and download again.Second, make a back up of old offline project then jot down all CPU-related parameters and then delete it from HW.Config. Then add new CPU--> apply new parameters-->Compile and download the hardware. If it works without error ,add the blocks and run the system. Note1:These test procedures should be followed by an experienced person who is aware of process-related risks. Note2: 6ES7416-2XN05-0AB0is successor of "6ES7416-2XK04-0AB0" that itself is the successor of "6ES7416-2XK02-0AB0". I hope these comments help you, Hamid Hosseini |
This contribution was helpful to
1 thankful Users |
Follow us on