(0)| 1/20/2015 2:42 AM | |
|
Posts: 1 Rating:
|
I need help with the web server, when i try to modify an output value exemple 1 to 0 nothing work. see my attachement file. thanks! |
Last edited by: Min_Moderator at: 1/20/2015 9:08 AMSplitted |
|
| 1/20/2015 6:58 AM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36484 Rating:
|
Here are screenshots.
AttachmentWebserver.zip (289 Downloads) |
| 1/20/2015 7:45 AM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36484 Rating:
|
A possibility of switching outputs which are used in the program is from the VM area. It is an OR-block before the corresponding output and sends it to this OR block an additional network Input. AttachmentWebserver variable NI.zip (293 Downloads) |
Follow us on