1/26/2015 10:08 PM | |
Posts: 87 Rating:
|
Hi. When you will insert a new Drive Object (check the attachment), you can modify the driver object type from Servo to Vector, then you can insert the telegram 352 for the Drive Object. In the Servo mode can not insert the telegram 352. But you can find the telegrams that are used in thisdocumentation, start onpg. 1805. Hope this help you. Regards.
AttachmentDriveObjectsType.pdf (1307 Downloads) |
1/28/2015 1:07 AM | |
Posts: 87 Rating:
|
Hi. Ok. I will try explanation for you. We can work with Servo mode and V\F without problem, but if we work with Servo and Vector mode, I think that is not good idea, because this situation is not good for the performance of the CU320. So, for me the best way for this, we can create a new project or delete all the Driver Objects and Create or Insert all Driver Objects in Vector mode. Please read the CU320_performance_sinamics-engineering-manual-v6-1. Which CF card do you have? Whithout performance expansion ou Whith performance expansion? In the attachment file there are a documentation CU320_performance_sinamics-engineering-manual-v6-1 and a example project, for make this tests I am using Starter V4.3.3.0 Hope this help you. Regards.
AttachmentDoc&Project.zip (662 Downloads) |
Follow us on