2/16/2015 6:38 PM | |
Posts: 8946 Rating:
|
Please check if scan time is too high. Also check if some Firmware update is available. |
2/16/2015 8:37 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello Farslan , Juergen is totally right.If all other event complains about OB33 , Execution time selected for this block (in Hw config) is too short compared to the code section to be executed.If the execution time is long enough, for test purpose when system is in shutdown bypass all code in OB33 with BEU and check the result.You have option of increasing the execution time of OB33 or distribute the codes over other OB3X with longer sampling time.It is also recommended to download OB80 in your CPUs and also avoid extensive loops in your critical time sections. Help on Event 3x02 Cause: I hope this helps, Hamid Hosseini |
This contribution was helpful to
1 thankful Users |
Follow us on