11/27/2015 11:17 AM | |
Joined: 3/2/2007 Last visit: 9/9/2025 Posts: 990 Rating:
|
this is strange. they should make a way to workaround this issue. |
... thank you ... |
|
11/27/2015 11:48 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
i don't understand the problem. TIA V13 SP1 project have no compatibility to Version lower then V13 SP1, this based on the new features which are released with this version (new PLC Device, new FW , new compiler, new compiler settings) To work with both versions TIA V13.0 and TIA V13 SP1 you can use the "Compatibility Mode" in TIA V13 SP1. Here you can build and configure project with V13 SP1 which can be used in V13.0 , but you can only use the feature set of the V13 in this V13.0 SP1 projects (no new device, no neW Function ...) To use the Compatibility mode you need a empty V13.0 project and don't update the project to v13 SP1. You can use your own V13 project or download the empty project from the CS Website: https://support.industry.siemens.com/cs/de/en/view/82169157 Regards |
11/27/2015 1:18 PM | |
Posts: 1529 Rating:
|
Tell me about it. I budget 5 days every time this happens. |
Follow us on