1/21/2016 5:11 PM | |
Posts: 4 Rating:
|
Hi I have LOGO OBA8 12/24Vdc and Logo soft confort V8 software, two Laptops DELL and TOSHIBA with windows 8.1, these OS not recognize the device via Ethernet, I tried do with all possible ways following tutorials and other suggestions I don-t know where is mistake, I will appreciate so much your aid. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/22/2016 9:16:26 AMNew subject after splitting |
|
1/21/2016 5:35 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
Have you installed the software as an administrator? Start you the software as an administrator? |
1/21/2016 6:12 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
In the attached video you will be shown whether the PC finds the logo on the network at all. If he finds the logo appears you the IP address and subnet mask. The logo and the PC must be on the same IP address space, subnet mask must be the same. AttachmentExample.wmv (359 Downloads) |
1/21/2016 6:25 PM | |
Posts: 4 Rating:
|
Yes I did, and windows and logo soft 8 start as administrator, however windows test reports NO ACCESS TO NET and LOGO test said NET OK |
1/21/2016 8:33 PM | |
Posts: 4 Rating:
|
I attached some screen prints
AttachmentLOGO GRAFICOS.docx (334 Downloads) |
1/21/2016 10:03 PM | |
Posts: 4 Rating:
|
Problem solved, thank you so much!! |
This contribution was helpful to
1 thankful Users |
Follow us on