1/28/2016 11:20 AM | |
Posts: 3 Rating:
|
I've attached the page from the help files. |
1/28/2016 12:12 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello , Indirect addressing with an index is not possible in Ladder diagrams for S7-300/400.You can try it for an S7-1200. The syntax you have tried is not suitable for STL , Normally for STL you works with absolute addresses and it is not easy to handle at the first try . The best and easiest solution in your case would be using SCL with the similar syntax you are using.Please refer to an old TIP on different programming languages regarding S7-300/400. Selection of proper programming LanguageYou can find a detailed STL<-->SCL comparison for similar applications (array-based) in the followoing topic: Arrays, DB and pointersI hope these comments help you, hdhosseini |
Last edited by: hdhosseini at: 1/28/2016 12:15:16 PM |
|
Follow us on