2/24/2016 7:06 AM | |
Posts: 7 Rating:
|
Good morning, Yesterday evening I had a bad surprise from my TIA 13 SP1 UP6. The icon of ASU disappeared and also the TIA link didn't start with many error. I decided to unistall all TIA 13 SP1 and restart the full installation. But (it is the 4th attempt) I'm not able to install it. I receive continuously the same error and I dont understan why. The log error is the following: 2016.02.24 06:52:40 - Year.Month.Day - Log start Before the installation I deactivated the antivirus and the firewall but the result is always the same. What I can do? I hope to not need to format my PC!!! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/24/2016 1:16:24 PMNew subject after splitting |
|
2/24/2016 7:20 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, first you should post the Logfile , not a extract from the log and not the summary Logfile. Have you more then one TIA Package installed? https://support.industry.siemens.com/cs/de/en/view/76325723 Regards |
Follow us on