3/7/2016 2:58 PM | |
Posts: 4 Rating:
|
I use TIA portal V11 SP2, but TC module 6ES7-231-5QD32-0XB0 isn't existing in catalog and also not included in update of catalogue that I downloaded how can I add this module to catalog as It can't be detected in Hardware Config. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/8/2016 3:42:47 PMNew subject after splitting |
|
3/7/2016 3:39 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello eng.tamer, Like I mentioned earlier, you will need TIA Portal V12 or later. Best regards, Wizard |
3/8/2016 8:28 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, You can migrate your TIA Portal v11 project to a TIA Portal v13 project. Edit: Here is a link: Sales/Delivery Release of the innovated S7-1200 Signal and Communication Modules The module is spare part compatible, so you can use without changing the hardware configuration. When you want to use the new functionality, you need to program the new number (Tia Portal v12) So it could be, that the module was programmed with ordernr. 6ES7 231-5QD30-0XB0 Best regards, Wizard |
Last edited by: Wizard at: 3/8/2016 8:33:02 AM |
|
Follow us on