4/4/2016 5:28 PM | |
Posts: 24 Rating:
|
Hi everyone, I have trouble using the "TIA v12 Trial" -which I have downloaded from Siemens site- going online and uploading the Project v11, using the Compatibility application also downloaded from Siemens site. Extrictly I could go online (Online Access), see the program blocks and its logic, but I could not save the Project in my computer or saw the Data Table, or do a Watch of the instant tag values. On the other hand, I can create a new Project without any limitation -as far as I can see-, selecting the CPU and creating tags, everything it's ok. I do not have any PLC Siemens to do some test, but it seems that if I have one I could download the Project an go online. Could you confirm to me if the limitation of doing an upload from the PLC is because I am working with a TRIAL or may be I am doing something wrong? I will appreciate your help very much. Regards, vperezb P.D.: I forgot to say that the CPU was a S7-1200. ------------------------------------------------------------------------------------------ |
Last edited by: vperezb at: 4/4/2016 9:25:10 PMLast edited by: Min_Moderator at: 4/5/2016 11:09:32 AMNew subject after splitting |
|
Follow us on