4/22/2016 10:21 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, organisation blocks(OB) are called when a error occurs. When they are not loaded, the CPU goes into STOP. For different errors the CPU calles different OB´s, e.g.program error OB121. In TIA there is a integrated System Diagnose, that generates all neccessary blocks when its activated. See the following application sample: System Diagnostics with S7-1500 and TIA Portal hope this helps, regards, |
FCK WAR! |
|
Follow us on